Keysight 89600 VSA .NET API
NonMbsfnRegionLength Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : NonMbsfnRegionLength Property


Glossary Item Box

Gets or sets the length of the non-MBSFN region in symbols within the MBSFN sub-frames.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property NonMbsfnRegionLength As Integer
C# 
public abstract int NonMbsfnRegionLength {get; set;}
C++/CLI 
public:
abstract property int NonMbsfnRegionLength {
   int get();
   void set (    int value);
}

Property Value

The minimum value is 1 and the maximum value is 2. The default value is 1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 15.00

See Also