Gets or sets the CSI-RS configuration.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property NonzeroCsiRsConfiguration As Integer |
| C# | |
|---|
public abstract int NonzeroCsiRsConfiguration {get; set;} |
| C++/CLI | |
|---|
public:
abstract property int NonzeroCsiRsConfiguration {
int get();
void set ( int value);
} |
Property Value
The default value is 0. The minimum value is 0 and the maximum value is 31.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 16.00
See Also