Gets or sets the number of antenna elements within each beam forming Antenna Group.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property NumberOfElementsPerAntennaGroup As Integer |
| C# | |
|---|
public abstract int NumberOfElementsPerAntennaGroup {get; set;} |
| C++/CLI | |
|---|
public:
abstract property int NumberOfElementsPerAntennaGroup {
int get();
void set ( int value);
} |
Property Value
The default value is 4. The minimum value is 2 and the maximum is 8.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 15.00
See Also