Gets or sets the number of antenna elements within each beam forming Antenna Group.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property NumberOfElementsPerAntennaGroupY As Integer |
| C# | |
|---|
public virtual int NumberOfElementsPerAntennaGroupY {get; set;} |
| C++/CLI | |
|---|
public:
virtual property int NumberOfElementsPerAntennaGroupY {
int get();
void set ( int value);
} |
Property Value
The default value is 4. The minimum value is 1 and the maximum is 64.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 22.20
See Also