Keysight 89600 VSA .NET API
PdcchBitVectorSelect Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : PdcchBitVectorSelect Property


Glossary Item Box

Gets or sets the PDCCH Bit Vector Selection to be applied.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PdcchBitVectorSelect As PdcchBitVectorSelectType
C# 
public abstract PdcchBitVectorSelectType PdcchBitVectorSelect {get; set;}
C++/CLI 
public:
abstract property PdcchBitVectorSelectType PdcchBitVectorSelect {
   PdcchBitVectorSelectType get();
   void set (    PdcchBitVectorSelectType value);
}

Property Value

The default value is PdcchBitVectorSelectType.Mapped

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also