Keysight 89600 VSA .NET API
PdcchScaleFactorIncrement Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : PdcchScaleFactorIncrement Property


Glossary Item Box

Gets or sets the per-subcarrier PDCCH scale factor increment in dB.

Syntax

Visual Basic (Declaration) 
Public Overridable Property PdcchScaleFactorIncrement As Double
C# 
public virtual double PdcchScaleFactorIncrement {get; set;}
C++/CLI 
public:
virtual property double PdcchScaleFactorIncrement {
   double get();
   void set (    double value);
}

Property Value

The default value is 1 dB. The minimum value is 0 dB and the maximum is 20 dB

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also