Keysight 89600 VSA .NET API
PdschBitVectorSelect Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : PdschBitVectorSelect Property


Glossary Item Box

Gets or sets the PDSCH Bit Vector Selection to be applied.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PdschBitVectorSelect As PdschBitVectorSelectType
C# 
public abstract PdschBitVectorSelectType PdschBitVectorSelect {get; set;}
C++/CLI 
public:
abstract property PdschBitVectorSelectType PdschBitVectorSelect {
   PdschBitVectorSelectType get();
   void set (    PdschBitVectorSelectType value);
}

Property Value

The default value is PdschBitVectorSelectType.Mapped.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also