Keysight 89600 VSA .NET API
PhichScaleFactor Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : PhichScaleFactor Property


Glossary Item Box

Gets or sets the per-subcarrier PHICH scale factor in dB.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PhichScaleFactor As Double
C# 
public abstract double PhichScaleFactor {get; set;}
C++/CLI 
public:
abstract property double PhichScaleFactor {
   double get();
   void set (    double value);
}

Property Value

The default value is 0 dB. The minimum value is -20 dB and the maximum is 20 dB

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also