Keysight 89600 VSA .NET API
PucchBitVectorSelect Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : PucchBitVectorSelect Property


Glossary Item Box

Gets or sets the PUCCH Bit Vector Selection to be applied.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PucchBitVectorSelect As PucchBitVectorSelectType
C# 
public abstract PucchBitVectorSelectType PucchBitVectorSelect {get; set;}
C++/CLI 
public:
abstract property PucchBitVectorSelectType PucchBitVectorSelect {
   PucchBitVectorSelectType get();
   void set (    PucchBitVectorSelectType value);
}

Property Value

The default value is PucchBitVectorSelectType.Mapped.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also