Keysight 89600 VSA .NET API
PuschHarqAckInformationSize Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : PuschHarqAckInformationSize Property


Glossary Item Box

Gets or sets the PUSCH HARQ-ACK Info Size.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PuschHarqAckInformationSize As Integer
C# 
public abstract int PuschHarqAckInformationSize {get; set;}
C++/CLI 
public:
abstract property int PuschHarqAckInformationSize {
   int get();
   void set (    int value);
}

Property Value

The default value is 0. The minimum value is 0 and the maximum is 11.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also