Gets or sets the minimum value of RA-RNTI Range
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property RARntiRangeMinValue As Integer |
| C# | |
|---|
public abstract int RARntiRangeMinValue {get; set;} |
| C++/CLI | |
|---|
public:
abstract property int RARntiRangeMinValue {
int get();
void set ( int value);
} |
Property Value
The default value is is 0. The minimum value is 0 and the maximum value is 60.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also