Keysight 89600 VSA .NET API
RBPowerDetectionThreshold Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : RBPowerDetectionThreshold Property


Glossary Item Box

Gets or sets the RB Power detection threshold in dB relative to the CRS power for Downlink measurement. Gets or sets the RB Power detection threshold in dB relative to the peak RB power for uplink measurement.

Syntax

Visual Basic (Declaration) 
Public Overridable Property RBPowerDetectionThreshold As Double
C# 
public virtual double RBPowerDetectionThreshold {get; set;}
C++/CLI 
public:
virtual property double RBPowerDetectionThreshold {
   double get();
   void set (    double value);
}

Property Value

The default value is -15 dB. The minimum value is -100dB and the maximum is 100 dB.

Remarks

RB whose power level fall below this threshold are not detected as active.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.20

See Also