Keysight 89600 VSA .NET API
ScmaNumberOfLayers Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : ScmaNumberOfLayers Property


Glossary Item Box

Gets or sets the number of layers for SCMA

Syntax

Visual Basic (Declaration) 
Public Overridable Property ScmaNumberOfLayers As Integer
C# 
public virtual int ScmaNumberOfLayers {get; set;}
C++/CLI 
public:
virtual property int ScmaNumberOfLayers {
   int get();
   void set (    int value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also