Keysight 89600 VSA .NET API
ScmaSpreadingFactor Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : ScmaSpreadingFactor Property


Glossary Item Box

Gets or sets the spreading factor (number of REs over which each symbol is spread) for SCMA

Syntax

Visual Basic (Declaration) 
Public Overridable Property ScmaSpreadingFactor As Integer
C# 
public virtual int ScmaSpreadingFactor {get; set;}
C++/CLI 
public:
virtual property int ScmaSpreadingFactor {
   int get();
   void set (    int value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also