Keysight 89600 VSA .NET API
SynchronizationSignalAntennaPort Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : SynchronizationSignalAntennaPort Property


Glossary Item Box

Gets or sets the P-SS/S-SS Antenna Port or Ports used for synchronization signal transmission.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SynchronizationSignalAntennaPort As SynchronizationSignalAntennaPortType
C# 
public abstract SynchronizationSignalAntennaPortType SynchronizationSignalAntennaPort {get; set;}
C++/CLI 
public:
abstract property SynchronizationSignalAntennaPortType SynchronizationSignalAntennaPort {
   SynchronizationSignalAntennaPortType get();
   void set (    SynchronizationSignalAntennaPortType value);
}

Property Value

The default value is SynchronizationSignalAntennaPortType.Port0.

Remarks

This is a downlink-only parameter.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also