Gets or sets the time scale factor.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property TimeScaleFactor As Double |
| C# | |
|---|
public abstract double TimeScaleFactor {get; set;} |
| C++/CLI | |
|---|
public:
abstract property double TimeScaleFactor {
double get();
void set ( double value);
} |
Property Value
The default value is 1.0. The minimum value is 1/16 and the maximum is 16.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also