Keysight 89600 VSA .NET API
UplinkDownlinkAllocation Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : UplinkDownlinkAllocation Property


Glossary Item Box

Gets or sets the Uplink/Downlink configuration type for TDD.

Syntax

Visual Basic (Declaration) 
Public Overridable Property UplinkDownlinkAllocation As UplinkDownlinkAllocationType
C# 
public virtual UplinkDownlinkAllocationType UplinkDownlinkAllocation {get; set;}
C++/CLI 
public:
virtual property UplinkDownlinkAllocationType UplinkDownlinkAllocation {
   UplinkDownlinkAllocationType get();
   void set (    UplinkDownlinkAllocationType value);
}

Property Value

The default value is UplinkDownlinkAllocationType.Allocation0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 14.00

See Also