Keysight 89600 VSA .NET API
UseAntenna Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : UseAntenna Property


Glossary Item Box

Gets or sets a value indicating whether to use the user-specified Tx antenna port as reference

Syntax

Visual Basic (Declaration) 
Public MustOverride Property UseAntenna As Boolean
C# 
public abstract bool UseAntenna {get; set;}
C++/CLI 
public:
abstract property bool UseAntenna {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Remarks

When set to true, the analyzer will use TXAntenna as the reference Tx antenna port. When set to false, the analyzer will automatically determine which Tx antenna port to use as the reference.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also