Keysight 89600 VSA .NET API
DeltaShift Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > Pucch Class : DeltaShift Property


Glossary Item Box

Gets or sets the higher layer parameter Delta_shift used for the determination of group number.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property DeltaShift As Integer
C# 
public abstract int DeltaShift {get; set;}
C++/CLI 
public:
abstract property int DeltaShift {
   int get();
   void set (    int value);
}

Property Value

The default value is 1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also