Keysight 89600 VSA .NET API
Pucch Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : Pucch Class

Glossary Item Box

The following tables list the members exposed by Pucch.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyActiveGets or sets a value indicating whether the channel is present in the signal. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyAllocationsGets the AllocationCollection associated with this channel. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyCW1McsIndexGets or sets the CW1 MCS index for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)20.0
Public PropertyCW1ModTypeGets or sets the modulation type for Code word 1 of the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyCW1PowerBoostGets or sets the per-subcarrier power boost in dB of Code word 1 of the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyCyclicShiftGets or sets the Cyclic Shift for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyDeltaShiftGets or sets the higher layer parameter Delta_shift used for the determination of group number.  —
Public PropertyDmrsCyclicShiftGets or sets the DRMS Alpha for the allocation/channel (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyDmrsGroupGets or sets the DRMS Group (u) of the allocation/channel (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyDmrsPowerBoostGets or sets the per-subcarrier DMRS power boost in dB for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyDmrsSeqGets or sets the DMRS sequence (v) for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyFormatGets or sets the PUCCH format for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyFrameIndexGets or sets the frame index for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyIncludeGets or sets a value indicating whether the channel is included in EVM calculations and shown in traces. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIncludeDmrsGets or sets a value indicating whether the PUCCH channel's DMRS is included in EVM calculations and shown in traces  —
Public PropertyIsAutoDetectPucchParametersEnabledGets or sets a value indicating whether PUCCH Format and NPUCCH1 are auto-detected.  —
Public PropertyIsAutoSyncEnabledGets or sets a value indicating whether synchronization slot is selected automatically. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsCyclicShiftCoupledGets or sets a value indicating whether all PUCCH allocations share the same Cyclic Shift.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsDmrsGroupCoupledGets or sets a value indicating whether all PUCCH allocations share the same DRMS Group (u).  —
Public PropertyIsDmrsPowerBoostCoupledGets or sets a value indicating whether all the allocations share the same DMRS Power Boost. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsFormatCoupledGets or sets a value indicating whether all PUCCH allocations share the same Format.  —
Public PropertyIsMcsIndexCoupledGets or sets a value indicating whether all the allocations share the same MCS index. (Inherited from Agilent.SA.Vsa.Lte.Channel)20.00
Public PropertyIsMirroringEnabledGets or sets a value indicating whether mirroring is used (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyIsModTypeCoupledGets or sets a value indicating whether all the allocations share the same mod type. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsNIdPucchEnabledGets or sets a value indicating whether the virtual Cell ID N_ID^PUCCH is set for the UL user  20.0
Public PropertyIsNPucch1CoupledGets or sets a value indicating whether all PUCCH allocations share the same n^(1).  —
Public PropertyIsNPucch3CoupledGets or sets a value indicating whether all PUCCH allocations share the same n^(3).  —
Public PropertyIsOSCoupledGets or sets a value indicating whether all PUCCH allocations share the same OS index.  —
Public PropertyIsPowerBoostCoupledGets or sets a value indicating whether all the allocations share the same Power Boost. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsRBEndCoupledGets or sets a value indicating whether all the allocations share the same RB End. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsRBStartCoupledGets or sets a value indicating whether all the allocations share the same RB Start. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsUseChannelParametersEnabledGets or sets a value indicating whether PUCCH group number, OS and cyclic shift are user-specified or determined from DMRS parameters  —
Public PropertyMcsIndexGets or sets the MCS index for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)20.0
Public PropertyModTypeGets or sets the modulation type for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyNameGets or sets the name of the allocation. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyNcs1Gets or sets N_cs^(1) used to determine PUCCH cyclic shift.  —
Public PropertyNIdPucchGets or sets the virtual Cell ID N_ID^PUCCH for the UL user  20.0
Public PropertyNPucch1Gets or sets n^(1)_PUCCH used to determine PUCCH cyclic shift for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyNPucch2Gets or sets n^(2) used to determine PUCCH cyclic shift.  —
Public PropertyNPucch3Gets or sets n^(3)_PUCCH used to determine PUCCH cyclic shift for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyNRb2Gets or sets N_RB^(2) used to determine PUCCH cyclic shift.  —
Public PropertyOSGets or sets the Orthogonal Sequence for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyPerAntennaEpreGets or sets the per-antenna EPRE in dB of the allocation/user. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)15.00
Public PropertyPowerBoostGets or sets the per-subcarrier power boost in dB for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyRBEndGets or sets the RB end for the allocation/channel (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyRBStartGets or sets the RB start for the allocation/channel (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertySlotEndGets or sets the Slot end for the allocation (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertySlotStartGets or sets the Slot Start for the allocation (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertySyncSlotGets or sets the slot to sync on. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also