Keysight 89600 VSA .NET API
IsNIdPucchEnabled Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > Pucch Class : IsNIdPucchEnabled Property


Glossary Item Box

Gets or sets a value indicating whether the virtual Cell ID N_ID^PUCCH is set for the UL user

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsNIdPucchEnabled As Boolean
C# 
public virtual bool IsNIdPucchEnabled {get; set;}
C++/CLI 
public:
virtual property bool IsNIdPucchEnabled {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 20.0

See Also