Keysight 89600 VSA .NET API
FreqHopNSb Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > Pusch Class : FreqHopNSb Property


Glossary Item Box

Gets or sets the higher layer number of sidebands parameter, N_sb.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FreqHopNSb As Integer
C# 
public abstract int FreqHopNSb {get; set;}
C++/CLI 
public:
abstract property int FreqHopNSb {
   int get();
   void set (    int value);
}

Property Value

The default value is 0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also