Keysight 89600 VSA .NET API
Pusch Class
Members  See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : Pusch Class


Glossary Item Box

The Pusch class contains properties and methods to control the behavior of LTE PUSCH channel.

Object Model

Pusch ClassAllocationCollection ClassAllocation ClassAllocation Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class Pusch 
   Inherits Channel
   Implements Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 
C# 
public abstract class Pusch : Channel, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  
C++/CLI 
public ref class Pusch abstract : public Channel, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also