Gets or sets a value indicating whether the PUSCH channel's DMRS is included in EVM calculations and shown in traces
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property IncludeDmrs As Boolean |
| C# | |
|---|
public abstract bool IncludeDmrs {get; set;} |
| C++/CLI | |
|---|
public:
abstract property bool IncludeDmrs {
bool get();
void set ( bool value);
} |
Property Value
The default value is true.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also