Keysight 89600 VSA .NET API
IsUsingCSFieldFromDci Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > Pusch Class : IsUsingCSFieldFromDci Property


Glossary Item Box

Gets or sets a value indicating whether n_DMRS^(2) and OCC are obtained from the cyclic shift field of DCI Format 0 or 4, or are specified directly.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsUsingCSFieldFromDci As Boolean
C# 
public abstract bool IsUsingCSFieldFromDci {get; set;}
C++/CLI 
public:
abstract property bool IsUsingCSFieldFromDci {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.0

See Also