Keysight 89600 VSA .NET API
LayerIndex Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > Pusch Class : LayerIndex Property


Glossary Item Box

Gets or sets the index of the layer of the MIMO signal that is being analyzed

Syntax

Visual Basic (Declaration) 
Public MustOverride Property LayerIndex As Integer
C# 
public abstract int LayerIndex {get; set;}
C++/CLI 
public:
abstract property int LayerIndex {
   int get();
   void set (    int value);
}

Property Value

The default value is 0. The minimum value is 0 and the maximum is 3.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.0

See Also