Gets or sets the virtual Cell ID N_ID^(csh_DMRS) for the UL user
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property NIdCyclicShiftDmrs As Integer |
| C# | |
|---|
public virtual int NIdCyclicShiftDmrs {get; set;} |
| C++/CLI | |
|---|
public:
virtual property int NIdCyclicShiftDmrs {
int get();
void set ( int value);
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 20.0
See Also