Keysight 89600 VSA .NET API
Enabled Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > RateMatchPattern Class : Enabled Property


Glossary Item Box

Gets or sets a value indicating whether this rate match pattern is active. When false, all other properties are ignored and no resource elements are masked.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Enabled As Boolean
C# 
public abstract bool Enabled {get; set;}
C++/CLI 
public:
abstract property bool Enabled {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also