The following tables list the members exposed by RateMatchPattern.
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | Enabled | Gets or sets a value indicating whether this rate match pattern is active. When false, all other properties are ignored and no resource elements are masked. | — |
![]() | IsDisposed | Gets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | SlotPatternPeriodicity | Gets or sets the length of the slot-pattern repetition window, expressed in LTE slots. | — |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | CreateObjRef | Creates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject) | — |
![]() | ForceRebuildKeyMap | This method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | GetLifetimeService | Retrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject) | — |
![]() | GetREMaskBitmap | Gets the 12-bit resource-element mask bitmap applied per PRB. | — |
![]() | GetResourceBlockBitmap | Gets the per-PRB selection bitmap across the carrier bandwidth. The bitmap length equals the number of frequency PRBs in the active carrier (for example, 100 for a 20 MHz LTE carrier). Bit i corresponds to frequency PRB index i; PRB 0 is the lowest-frequency PRB. A bit value of 1 means the rate match pattern is applied to that PRB; 0 means the PRB is untouched and every RE in it carries data. | — |
![]() | GetSlotPatternBitmap | Gets the slot-activity bitmap within one SlotPatternPeriodicity window. The bitmap length equals the numeric value of SlotPatternPeriodicity. The MSB corresponds to the first slot of the repeating window; the LSB corresponds to the last. A bit value of 1 means the rate match pattern is active during that slot of the cycle; 0 means it is inactive during that slot. | — |
![]() | GetSymbolBitmap | Gets the per-symbol selection bitmap within a single LTE slot. The bitmap is always 7 bits (MSB = symbol 0, LSB = symbol 6). A bit value of 1 means the rate match pattern is active during that symbol. | — |
![]() | InitializeLifetimeService | Obtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | SetREMaskBitmap | Sets the 12-bit resource-element mask bitmap applied per PRB. | — |
![]() | SetResourceBlockBitmap | Sets the per-PRB selection bitmap. | — |
![]() | SetSlotPatternBitmap | Sets the slot-activity bitmap within one SlotPatternPeriodicity window. | — |
![]() | SetSymbolBitmap | Sets the per-symbol selection bitmap within a single LTE slot. | — |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | PropertyChanged | Occurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | PropertyInfoChanged | Occurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | RemotePropertyChanged | Occurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | RemotePropertyInfoChanged | Occurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | 14.00 |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||