Keysight 89600 VSA .NET API
GetREMaskBitmap Method
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > RateMatchPattern Class : GetREMaskBitmap Method


Glossary Item Box

Gets the 12-bit resource-element mask bitmap applied per PRB.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function GetREMaskBitmap() As BitArray
C# 
public abstract BitArray GetREMaskBitmap()
C++/CLI 
public:
abstract BitArray^ GetREMaskBitmap(); 

Return Value

The current RE mask bitmap (12 elements; index 0 = RE0 = MSB).

Remarks

The returned System.Collections.BitArray has length 12. Element 0 corresponds to RE index 0 (lowest frequency in the PRB, MSB); element 11 corresponds to RE index 11 (highest frequency in the PRB, LSB). A true element means PxSCH data is present in that RE; a false element means the RE is "missing" (zero in U-Plane, excluded from demodulation, EVM, and decoding). Default is all 12 bits false (0x000; all REs are punctured by default — use SetREMaskBitmap to mark individual REs as data-carrying, e.g. #b010101010101 for alternating REs). See O-RAN.WG4.TS.CUS.0 §7.5.3.5 (value range: {0000 0000 0000b – 1111 1111 1111b}).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also