Keysight 89600 VSA .NET API
GetResourceBlockBitmap Method
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > RateMatchPattern Class : GetResourceBlockBitmap Method


Glossary Item Box

Gets the per-PRB selection bitmap across the carrier bandwidth. The bitmap length equals the number of frequency PRBs in the active carrier (for example, 100 for a 20 MHz LTE carrier). Bit i corresponds to frequency PRB index i; PRB 0 is the lowest-frequency PRB. A bit value of 1 means the rate match pattern is applied to that PRB; 0 means the PRB is untouched and every RE in it carries data.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function GetResourceBlockBitmap() As BitArray
C# 
public abstract BitArray GetResourceBlockBitmap()
C++/CLI 
public:
abstract BitArray^ GetResourceBlockBitmap(); 

Return Value

The current resource block selection bitmap.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also