Keysight 89600 VSA .NET API
GetSlotPatternBitmap Method
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > RateMatchPattern Class : GetSlotPatternBitmap Method


Glossary Item Box

Gets the slot-activity bitmap within one SlotPatternPeriodicity window. The bitmap length equals the numeric value of SlotPatternPeriodicity. The MSB corresponds to the first slot of the repeating window; the LSB corresponds to the last. A bit value of 1 means the rate match pattern is active during that slot of the cycle; 0 means it is inactive during that slot.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function GetSlotPatternBitmap() As BitArray
C# 
public abstract BitArray GetSlotPatternBitmap()
C++/CLI 
public:
abstract BitArray^ GetSlotPatternBitmap(); 

Return Value

The current slot-pattern bitmap.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also