| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function GetSymbolBitmap() As BitArray | |
| C# | |
|---|---|
public abstract BitArray GetSymbolBitmap() | |
| C++/CLI | |
|---|---|
public: abstract BitArray^ GetSymbolBitmap(); | |
Return Value
The current per-symbol selection bitmap.Valid bit-index range depends on the cyclic-prefix length of the analyzed signal:
- Normal cyclic prefix (or auto-detected normal CP): bits 0..6 are valid (7 OFDM symbols per slot).
- Extended cyclic prefix (or auto-detected extended CP): bits 0..5 are valid (6 OFDM symbols per slot); bit 6 has no effect.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)