Keysight 89600 VSA .NET API
InputDataDomain Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.Lte Namespace > ConfigurationResult Class : InputDataDomain Property


Glossary Item Box

Gets the configured input data domain.

Syntax

Visual Basic (Declaration) 
Public ReadOnly Property InputDataDomain As InputDataDomain
C# 
public InputDataDomain InputDataDomain {get;}
C++/CLI 
public:
property InputDataDomain InputDataDomain {
   InputDataDomain get();
}

Remarks

The configured input data domain can be either InputDataDomain.Time or InputDataDomain.Ofdm. This information is got from InputDataDomain provided by ConfigureWithVsaSetupFile(string fileName, CalculationControl calculationControl).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also