Keysight 89600 VSA .NET API
ConfigurationResult Class Members
See Also  Properties 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.Lte Namespace : ConfigurationResult Class

Glossary Item Box

The following tables list the members exposed by ConfigurationResult.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorConfigurationResult ConstructorInitializes a new instance of the ConfigurationResult class.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyCyclicPrefixLengthGets the configured cyclic prefix length.  —
Public PropertyInputDataDomainGets the configured input data domain.  —
Public PropertyRequiredInputDataPointsGets the total number of input data samples the user must supply in order to satisfy the configured measurement.  —
Public PropertyRequirementsForOfdmDomainInputDataGets a reference to the requirements for the ofdm domain input data.  —
Public PropertyRequirementsForTimeDomainInputDataGets a reference to the requirements for the time domain input data.  —
Public PropertyResultLengthInSlotsGets the demodulation result length defined in number of slots.  —
Public PropertySignalFormatGets the configured signal format.  —
Public PropertyStatusGets the overall status after the configuration.  —
Public PropertyStatusMessagesGets the collection of all the status messages after the configuration.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also