Keysight 89600 VSA .NET API
Status Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.Lte Namespace > ConfigurationResult Class : Status Property


Glossary Item Box

Gets the overall status after the configuration.

Syntax

Visual Basic (Declaration) 
Public ReadOnly Property Status As OverallStatus
C# 
public OverallStatus Status {get;}
C++/CLI 
public:
property OverallStatus Status {
   OverallStatus get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also