Keysight 89600 VSA .NET API
RequirementsForOfdmDomainInputData Class Members
See Also  Properties 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.Lte Namespace : RequirementsForOfdmDomainInputData Class

Glossary Item Box

The following tables list the members exposed by RequirementsForOfdmDomainInputData.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorRequirementsForOfdmDomainInputData ConstructorInitializes a new instance of the RequirementsForOfdmDomainInputData class.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyFirstSubcarrierIndexGets the required first subcarrier index. Valid subcarrier index range starts at value 0.  —
Public PropertyFirstSymbolIndexGets the required first symbol index. Valid symbol index range starts at value 0.  —
Public PropertyNumberOfSubcarriersGets the required number of subcarriers.  —
Public PropertyNumberOfSymbolsGets the required number of symbols.  —
Public PropertySubcarrierSpacingGets the required subcarrier spacing with unit of Hz.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also