Keysight 89600 VSA .NET API
SubcarrierSpacing Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.Lte Namespace > RequirementsForOfdmDomainInputData Class : SubcarrierSpacing Property


Glossary Item Box

Gets the required subcarrier spacing with unit of Hz.

Syntax

Visual Basic (Declaration) 
Public ReadOnly Property SubcarrierSpacing As Double
C# 
public double SubcarrierSpacing {get;}
C++/CLI 
public:
property double SubcarrierSpacing {
   double get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also