Keysight 89600 VSA .NET API
RequirementsForTimeDomainInputData Class Members
See Also  Properties 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.Lte Namespace : RequirementsForTimeDomainInputData Class

Glossary Item Box

The following tables list the members exposed by RequirementsForTimeDomainInputData.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorRequirementsForTimeDomainInputData ConstructorInitializes a new instance of the RequirementsForTimeDomainInputData class.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyDelayPointsGets the number of input data pre-settling (delay) samples incurred during the configured measurement.  —
Public PropertySampleRateGets the required sample rate for time domain input data with unit of Hz.  —
Public PropertySettlePointsGets the sum total of input data settling samples the user must supply in order to satisfy the configured measurement.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also