| Visual Basic (Declaration) | |
|---|---|
Public ReadOnly Property SettlePoints As Long | |
| C# | |
|---|---|
public long SettlePoints {get;} | |
This calculated value represents the sum total of any additional pre-settling (delay) + post-settling samples required to settle the measurement filtering used in the demodulation process. Note the calculated number of input data pre-settling (delay) samples is returned separately as DelayPoints. To summarize, SettlePoints = DelayPoints + post-settling sample points.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)