Keysight 89600 VSA .NET API
DownlinkUserCollection Class
Members  See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace : DownlinkUserCollection Class


Glossary Item Box

The DownlinkUserCollection class contains properties and methods to manipulate a collection of NB-IoT DownlinkUser objects.

Object Model

DownlinkUserCollection ClassDownlinkUser ClassDownlinkUser Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class DownlinkUserCollection 
   Inherits Agilent.SA.Vsa.NBIot.UserCollection(Of DownlinkUser)
   Implements Agilent.SA.Vsa.ICollectionBase, Agilent.SA.Vsa.ICollectionBase(Of DownlinkUser), Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyCollectionChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also