| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property EqualizerTrainingMode As EqualizerTrainingModeType | |
| C# | |
|---|---|
public abstract EqualizerTrainingModeType EqualizerTrainingMode {get; set;} | |
| C++/CLI | |
|---|---|
public: abstract property EqualizerTrainingModeType EqualizerTrainingMode { EqualizerTrainingModeType get(); void set ( EqualizerTrainingModeType value); } | |
Property Value
The default value is EqualizerTrainingModeType.ZF.Determines whether equalizer coefficients are calculated based on the standard Least Squares method or non-standard Zero Forcing method.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)