Keysight 89600 VSA .NET API
MeasurementExtension Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace : MeasurementExtension Class

Glossary Item Box

The following tables list the members exposed by MeasurementExtension.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAnalysisStartBoundaryGets or sets the analysis start boundary.  —
Public PropertyAntennaDetectionThresholdGets or sets the antenna detection threshold in dB relative to the reference path.  —
Public PropertyCellIdentityGets or sets the Physical Layer Cell ID.  —
Public PropertyCellIdModeGets or sets whether the Cell ID is auto-detected or manually specified  —
Public PropertyCrsScaleFactorGets or sets the per-subcarrier CRS scale factor in dB. Only applicable to in-band signals.  —
Public PropertyDownlinkUsersGets the collection of downlink users (NPDSCH).  —
Public PropertyEqualizerTrainingGets or sets the equalizer training type as being Off or RS-based or RS+Data based.  —
Public PropertyEqualizerTrainingModeGets or sets the equalizer training mode (Uplink only)  —
Public PropertyEqualizerTrainingMovingAverageLengthGets or sets the EQ Moving Average Filter Length in number of RS subcarriers.  —
Public PropertyEutraCellIdentityGets or sets the Cell ID of the LTE carrier.  —
Public PropertyEutraChannelBandwidthGets or sets the bandwidth of the LTE carrier.  —
Public PropertyEutraControlRegionSizeGets or sets the control region size of the LTE carrier.  —
Public PropertyEutraRbOffsetGets or sets the resource block offset of the narrowband carrier within the LTE carrier.  —
Public PropertyEvmMinimizationGets or sets what EVM minimization method is employed.  —
Public PropertyIsAmplitudeIncludedInEvmMinimizationGets or sets a value indicating whether EVM Minimization of Amplitude is enabled.  —
Public PropertyIsCoarseFrequencyEstimationEnabledGets or sets a value indicating whether coarse frequency offset compensation is enabled for uplink.  24.00
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsEqualizerChannelFrequencyResponseNormalizedGets or sets a value indicating whether the MIMO Eq Chan Freq Resp trace is normalized to the reference path.  —
Public PropertyIsEqualizerTrainingMovingAverageEnabledGets or sets a value indicating whether a moving average of the NRS subcarriers is employed in equalizer training.  —
Public PropertyIsEvmReportedInDBGets or sets a value indicating whether EVM results are reported in dB.  —
Public PropertyIsFrequencyIncludedInEvmMinimizationGets or sets a value indicating whether EVM Minimization of frequency is enabled.  —
Public PropertyIsFrequencyMirroredGets or sets a value indicating whether demod will mirror the frequency spectrum.  —
Public PropertyIsHalfSubcarrierShiftEnabledGets or sets a value indicating whether half subcarrier shift is enabled.  —
Public PropertyIsInactiveEnabledGets or sets a value indicating whether non-allocated resource elements or non-NBIoT resource elements are shown in trace displays.  —
Public PropertyIsIQOffsetIncludedInEvmMinimizationGets or sets a value indicating whether EVM Minimization of IQ Offset is enabled.  24.00
Public PropertyIsMulticarrierFilterEnabledGets or sets a value indicating whether a multi-carrier filter will be applied.  —
Public PropertyIsNarrowerFilterStopbandEnabledGets or sets a value indicating whether to use a narrower filter stop band when IsMulticarrierFilterEnabled = true.  —
Public PropertyIsNpbchEnabledGets or sets a value indicating whether NPBCH is enabled in trace displays and included in overall EVM calculation.  —
Public PropertyIsNpdcchEnabledGets or sets a value indicating whether NPDCCH is enabled in trace displays and included in overall EVM calculation.  —
Public PropertyIsNprsActiveGets or sets a value indicating whether NPRS is present in the signal.  24.00
Public PropertyIsNprsBitmapConfiguredGets or sets a value indicating whether the nprs bitmap parameter is configured.  24.00
Public PropertyIsNprsEnabledGets or sets a value indicating whether NPRS is enabled in trace displays and included in overall EVM calculation.  24.00
Public PropertyIsNpssEnabledGets or sets a value indicating whether NPSS is enabled in trace displays and included in overall EVM calculation.  —
Public PropertyIsNrsEnabledGets or sets a value indicating whether NRS is enabled in trace displays and included in overall EVM calculation.  —
Public PropertyIsNsssEnabledGets or sets a value indicating whether NSSS is enabled in trace displays and included in overall EVM calculation.  —
Public PropertyIsNtmSignalGets or sets a value indicating whether the signal is an N-TM signal.  —
Public PropertyIsNtmSignalAutoDetectGets or sets a value indicating whether auto detection is enabled for detecting whether the signal is an N-TM signal.  —
Public PropertyIsPowerBoostNormalizedGets or sets a value indicating whether channels' power levels are normalized to 0dB in traces.  —
Public PropertyIsTimingIncludedInEvmMinimizationGets or sets a value indicating whether EVM Minimization of Timing is enabled.  —
Public PropertyIsTriggerPresentGets or sets a value indicating whether a trigger has been provided to locate the beginning of the frame or burst.  24.20
Public PropertyLayerDecodingGets or sets the decoding to apply to channels that have undergone precoding.  —
Public PropertyLinkDirectionGets or sets the link direction.  —
Public PropertyMeasureIntervalSlotsGets or sets the measurement interval as an integer number of slots.  —
Public PropertyMeasureIntervalSymbolsGets or sets the measurement interval as an integer number of symbols.  —
Public PropertyMeasureOffsetSlotsGets or sets the measurement offset expressed as an integer number of slots.  —
Public PropertyMeasureOffsetSymbolsGets or sets the measurement offset expressed as an integer number of symbol times.  —
Public PropertyNpbchBitVectorSelectGets or sets the NPBCH decoding to be applied.  —
Public PropertyNpbchPhaseRotationEnabledGets or sets a value indicating whether NPBCH phase rotation is enabled.  25.20
Public PropertyNpbchScaleFactorGets or sets the per-subcarrier NPBCH scale factor in dB.  24.00
Public PropertyNpdcchScaleFactorGets or sets the per-subcarrier NPDCCH scale factor in dB.  —
Public PropertyNpdschBitVectorSelectGets or sets the NPDSCH decoding to be applied.  24.00
Public PropertyNprsIdGets or sets the NPRS ID.  24.00
Public PropertyNprsScaleFactorGets or sets the per-subcarrier NPRS scale factor in dB.  24.00
Public PropertyNprsSequenceInfoGets or sets the nprs SequenceInfo higher-layer parameter. Only applicable when OperationMode is in-band.  24.00
Public PropertyNprsSequenceInfoAutoGets or sets a value indicating whether the nprs SequenceInfo higher-layer parameter is determined from EutraRbOffset or specified manually.  24.00
Public PropertyNpssScaleFactorGets or sets the per-subcarrier NPSS scale factor in dB.  —
Public PropertyNpuschAllSymbolsGets or sets a value indicating whether the higher layer parameter NpuschAllSymbols parameter is set to true.  24.00
Public PropertyNpuschBitVectorSelectGets or sets how much decoding to apply to NPUSCH.  24.00
Public PropertyNpuschParametersAutoDetectGets or sets a value indicating whether NpuschToneNumber, NpuschSubcarrierSpacing, and NpuschSubcarrierOffset are auto detected.  24.00
Public PropertyNpuschSubcarrierOffsetGets or sets the NPUSCH subcarrier offset.  24.00
Public PropertyNpuschSubcarrierSpacingGets or sets the NPUSCH subcarrier spacing.  24.00
Public PropertyNpuschToneNumberGets or sets the number of tones for NPUSCH.  24.00
Public PropertyNrsReferenceAntennaGets or sets the TX antenna port to be used as the reference antenna port.  —
Public PropertyNrsScaleFactorGets or sets the per-subcarrier NRS scale factor in dB.  —
Public PropertyNsssScaleFactorGets or sets the per-subcarrier NSSS scale factor in dB.  —
Public PropertyNumberOfEutraCrsAntennasGets or sets the number of CRS antenna ports that the LTE carrier uses.  —
Public PropertyNumberOfNrsAntennasGets or sets the number of NRS antenna ports that the narrowband carrier uses.  —
Public PropertyOperationModeGets or sets the downlink operation mode.  —
Public PropertyRBAutoDetectModeGets or sets a value indicating the type of RB Auto Detection to perform.  —
Public PropertyRBPowerDetectionThresholdGets or sets the RB Power detection threshold in dB relative to the NRS power for Downlink measurement.  —
Public PropertyResultLengthGets or sets the result length (in slots).  —
Public PropertyResultLengthAutoGets or sets a value indicating whether ResultLength is determined based on other parameters (uplink-only).  24.00
Public PropertyScaleFactorAutoDetectGets or sets a value indicating whether downlink channel scale factors are auto-detected.  —
Public PropertySymbolTimeAdjustmentGets or sets where within the cyclic prefix IFFT begins as a percentage of the IFFT duration.  —
Public PropertySymbolTimeAdjustmentModeGets or sets the Symbol Time Adjust mode.  —
Public PropertySynchronizationSignalAntennaPortGets or sets the NPSS/NSSS Antenna Port or Ports used for synchronization signal transmission.  —
Public PropertySynchronizationTypeGets or sets the channel used for synchronization.  —
Public PropertyUplinkOperationModeGets or sets the uplink operation mode.  —
Public PropertyUplinkUsersGets the collection of uplink users.  24.00
Public PropertyUseNrsReferenceAntennaGets or sets a value indicating whether to use a specific Tx antenna port as reference for power and other metrics.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public Methodstatic (Shared in Visual Basic)CastToExtensionTypeThis method casts the supplied object to the MeasurementExtension type. Some tools are unable to use the generic methods provided on Agilent.SA.Vsa.Measurement class so this is provided as an alternative.  —
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public Methodstatic (Shared in Visual Basic)ExtensionTypeReturns the type for instances this measurement extension. Some tools are unable to use the generic methods provided on Agilent.SA.Vsa.Measurement class so this is provided as an alternative.  —
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetDownlinkSubframeChannelAssignmentsGets a vector that specifies the channel that each subframe contains.  —
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodGetNprsBitmapGets the nprs bitmap parameter as a list of integers.  24.00
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodPresetPreset all measurement attributes to their defaults, sets LinkDirection to Downlink, and sets operation mode to downlink.  —
Public MethodPresetUplinkPresets all measurement attributes to their default and sets the LinkDirection to uplink.  24.00
Public MethodSetDownlinkSubframeChannelAssignmentsSets a vector that specifies the channel that each subframe contains.  —
Public MethodSetNprsBitmapSets the nprs bitmap parameter to configure which subframes contain NPRS.  24.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also