Keysight 89600 VSA .NET API
EutraCellIdentity Property
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace > MeasurementExtension Class : EutraCellIdentity Property


Glossary Item Box

Gets or sets the Cell ID of the LTE carrier.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property EutraCellIdentity As Integer
C# 
public abstract int EutraCellIdentity {get; set;}
C++/CLI 
public:
abstract property int EutraCellIdentity {
   int get();
   void set (    int value);
}

Remarks

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also