Keysight 89600 VSA .NET API
EutraControlRegionSize Property
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace > MeasurementExtension Class : EutraControlRegionSize Property


Glossary Item Box

Gets or sets the control region size of the LTE carrier.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property EutraControlRegionSize As Integer
C# 
public abstract int EutraControlRegionSize {get; set;}
C++/CLI 
public:
abstract property int EutraControlRegionSize {
   int get();
   void set (    int value);
}

Property Value

Valid range: 1-3 symbols

Remarks

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also