Keysight 89600 VSA .NET API
IsAmplitudeIncludedInEvmMinimization Property
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace > MeasurementExtension Class : IsAmplitudeIncludedInEvmMinimization Property


Glossary Item Box

Gets or sets a value indicating whether EVM Minimization of Amplitude is enabled.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsAmplitudeIncludedInEvmMinimization As Boolean
C# 
public abstract bool IsAmplitudeIncludedInEvmMinimization {get; set;}
C++/CLI 
public:
abstract property bool IsAmplitudeIncludedInEvmMinimization {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also