Keysight 89600 VSA .NET API
IsNtmSignal Property
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace > MeasurementExtension Class : IsNtmSignal Property


Glossary Item Box

Gets or sets a value indicating whether the signal is an N-TM signal.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsNtmSignal As Boolean
C# 
public abstract bool IsNtmSignal {get; set;}
C++/CLI 
public:
abstract property bool IsNtmSignal {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Remarks

When set to true, the demodulator will assume the signal is an N-TM signal. Note this parameter is ignored when IsNtmSignalAutoDetect = true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also