Keysight 89600 VSA .NET API
NpuschAllSymbols Property
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace > MeasurementExtension Class : NpuschAllSymbols Property


Glossary Item Box

Gets or sets a value indicating whether the higher layer parameter NpuschAllSymbols parameter is set to true.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property NpuschAllSymbols As Boolean
C# 
public abstract bool NpuschAllSymbols {get; set;}
C++/CLI 
public:
abstract property bool NpuschAllSymbols {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

Affects NPUSCH resource elements that overlap SRS for an in-band NB-IoT signal.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also