Gets or sets the RB Power detection threshold in dB relative to the NRS power for Downlink measurement.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property RBPowerDetectionThreshold As Single |
| C# | |
|---|
public abstract float RBPowerDetectionThreshold {get; set;} |
| C++/CLI | |
|---|
public:
abstract property float RBPowerDetectionThreshold {
float get();
void set ( float value);
} |
Property Value
The default value is -15 dB. The minimum value is -100dB and the maximum is 100 dB.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also