Keysight 89600 VSA .NET API
UseNrsReferenceAntenna Property
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace > MeasurementExtension Class : UseNrsReferenceAntenna Property


Glossary Item Box

Gets or sets a value indicating whether to use a specific Tx antenna port as reference for power and other metrics.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property UseNrsReferenceAntenna As Boolean
C# 
public abstract bool UseNrsReferenceAntenna {get; set;}
C++/CLI 
public:
abstract property bool UseNrsReferenceAntenna {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Remarks

When set to true, the demodulator will use NrsReferenceAntenna as the reference Tx antenna port. When set to false, the demodulator will automatically determine which Tx antenna port to use as the reference.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also